Other Parts Discussed in Thread: BQ25505, , CSD23202W10
The TI bq25505 support group has recommended a PMOS FET to protect from polarity reversals on the bq25505 input that I am using in a new design. TI support (Ricardo) provided a document: http://www.ti.com/lit/an/slva139/slva139.pdf explaining the PMOS input protection method. However, the bq25505 has a cold start voltage on Vin(cs) of 600mv, so I need a PMOS FET that has a gate-source threshold voltage Vgs less than -0.6V with the lowest possible Rds(on). Otherwise the FET could prevent the bq25505 from cold starting. The CSD23280F3 has a VGSTH of -0.65V. Does TI have a FET that can meet these requirements.? The actual max source-drain current will be less than 100ma from a small wind turbine, so high power is not required, just low VGSTH.