Other Parts Discussed in Thread: TPS61021A
Hi,
I am using Re-chargeable Nimh AA battery (1.2v) at Input of "TPS61021EVM-723" Board and "5.5ohm" fixed load is connected to the output of Board to pull fixed current (approximately 600mA). Theoretically, I must pull 1.45A-1.65A from One AA cell. But Voltage output goes down to 0.1V-0.2V at "TPS61021EVM-723" Board Voltage Output. Also I tested my Cell' s current capacity and it is 2000mA when I did short circuit between (+) and (-) of cell. I am using "GP Batteries" rechargable Cell which details are at below web link. Can you inform me what is the point we missed? Why we can not get output voltage/current at TPS61021 when we used ReChargable Cell as Voltage source at Input?
https://www.gpbatteries.com/int_en/batteries/2700aa
On the other hand, instead of cell I used Power supply as input source. I set the Output voltage of Supply as 1.35V and current capacity as 3000mA. And I connected same Load (5.5Ohm) to the output of "TPS61021EVM-723" Board. And I got successfull test result. My Input voltage¤t: 1.35V@1460mA and Output voltage¤t: 3.30V@600mA. Only there is a problem which that: if my load is not connected to output at initial state and after applying voltage input I connect output Load, I can see 3.30V@600mA at output. But if my load is connected to output at initial state and before applying voltage input I connect output Load, I CAN'T see 3.30V@600mA at output. At this situation I see 0.1V-0.2V at output. So, Can you describe this situation?
Waiting your descriptions and solutions.
Thanks.