Hi there,
I have 2 questions with using this device.
1. The RC snubber network suggested by the reference design doc (SNVS397E –SEPTEMBER 2005–REVISED NOVEMBER 2016) on pg 23 suggests a 1 Watt resistor for Rs. IE: 10 Ω, 1 W, 1206
Is this 1W value really sufficient - surely the full output voltage (e.g 5V) is seen by this resistor? Meaning a 0.5 A current drop and 2.5 Watts?
2. Does the device require a minimum load, I have been using the reference design in the PDF and it mentions a minimum load current of 250mA on pg 17 - does this mean for this design to work the output at Vout must always have 250 mA minimum?
Thanks in advance for your help!