Other Parts Discussed in Thread: UCC28C42, PMP10833
Hi,
For a flyback converter with UCC28C42 IC designed for the input range of 30-212VAC and output of 14VDC/6A, What will be the output voltage for the following inputs?
1. Vin = 25VAC, load=2A, Vout=?
2. Vin = 20VAC, load= 1A, Vout=?
3. Vin= 15VAC, load= 1A, Vout=?
4. Vin=10VAC, load=1A, Vout=?
Please some one help me. You can refer the design with you have for the other operating limits and can check the output for lower input level than the designed range.
Thanks and Regards,
Ajmal T