This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950: incorrect arxl1_apga_ctl reg description

Part Number: TPS65950

In the TPS65950 OMAP document ("TPS65950 OMAP(TM) Power Management and System Companion Device ES 1.2 TRM (Rev. G)" at  http://www.ti.com/product/TPS65950/technicaldocuments), the ARXL1_APGA_CTL Register (table 14-38 on page 758) definition shows 5 bits (7:3) for the ARXL1_GAIN_SET field, but the description only goes to 4 bits (0xF). Does anybody know the correct interpretation of the ARXL1_GAIN_SET field? (i.e. should I just ignore bit 7, or is bit 3 the one to be ignore? Or should it really be a scale of 1dB per number (i.e. 0x0 is 12dB, 0x1 is 11dB, 0x2 is 10db, ... 0x1F is -18dB) instead of 2dB(i.e. the current, incorrect description has it as 0x0 is 12dB, 0x1 is 10dB, 0x2 is 8dB, ... 0xF is -18dB)?