This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
We recommend sot-23 TLV758p and TLV755 to customer. But customer wonder about the thermal resistance of those IC.
They will have 1.5W loss with 500mA load current but only last 1 second. Then repeat the short pulse after several hours. Will the LDO have some effects with the 1 second pulse? It will exceed 150 degree C.
Any other SOT23 LDO recommend for this?
Thanks.
Best regards,
Sammi
Hi Sammi,
Of these, the TLV758P has the best thermal performance for the SOT-23 package. This has a TJA 176.9C/W. With 1.5W of power dissipation, this is a 265.35C (1.5x176.9) rise above ambient.
1s is a long time for this condition and the LDO will definitely thermally shutdown.
There is no SOT-23 LDO that can handle this.
A better solution might be something like the TPS73701DRB which has a TJA of 49.5C/W which would yield a 74.25C rise above ambient.
I hope this helps.