This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24171: BATDRV

Part Number: BQ24171

Hi,

We are designing a circuit that include a lithium battery charge (BQ24171RGYT and BQ27441DRZR-G1A).

The circuit for the charger is very similar to the one shown in BQ24171EVM-706-15V (for 1 cell). It includes the “Battery discharge MOSFET gate driver output” BATDRV mosfet.

The circuit needs to provide the option to disconnect the battery during storage.

One option is using a bidirectional mosfet circuit next the battery connector (it will be triggered externally by a tiny TACT switch, active low).

Question:

Can we use the BATDRV mosfet to disconnect the battery from the load? Using an AND circuit (inputs # BATDRV and TACT switch associated to a latching circuit).

Or can you advice other way to do it? No much pcb real state is available.

Thank you in advance