Other Parts Discussed in Thread: PMP22210, UCC28881
Dear Team
I'm a student from switzerland and i would like to design a buck converter (without isolated output) with the ucc28710 chip. My design should work in range of 85VAC to 275VAC input and the output should be 3.3VDC by a current around 100mA. Is the ucc28710 a ideal device for a low cost, high efficiency AC/DC converter?
The datasheet from ucc28710 treated only isolated topologies, so i found your reference design for a buck converter. Do you have any datasheets who treat non isolated topologies?
Next i simulated the reference design below with the ucc28710 transient model in the simulation programm TINA9, but it doesen't work. Even the start up proced doesn't work. What could be my failure?
After that i bought some ucc28710 to built the reference desgin. With a DC input (up to 110V) works nothing. Then i replaced the DC input with a AC input and the diode recifier with a bridge recifier. After that i saw the start up proced by a input voltage of 20VAC(make sense). Why it doesen't work with a DC input?
How can i influence the output voltage?
Best Regards
Sandro