I am working on a design using the LM5112 on a dual-supply (+6 and -8V) application. I would like to connect the IN_REF pin to ground to allow for simple TTL control. The recommended operating conditions specify that VCC to IN_REF must be less than 14V (it is) and that VCC to VEE must be less than 14V (it also is, barely).
My concern is the absolute maximum ratings specify that IN_REF to VEE must be less than 5V which would be violated in this design. It's strange that there is no recommended operating condition regarding the IN_REF-VEE voltage.
I learned about the LM5112 from another design where it is successfully being used with a VEE of -8V without apparent issue. Can you clarify if this absolute maximum rating is real? What is the recommended operating voltage of IN_REF-VEE?