This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to download TPS650942.json file? I follow the TPS650941EVM-116 guide and answer the request but still fail to download
Hello Antares,
I have just provided you access. You should get an email link in the next hour or so to download the file. It will be available through TI's mySecure software portal. To access mySecure, you can also log in to ti.com, click on your name to access your myTI account, and then click on the mySecure software link in the bottom left corner.
Please let us know if you have any issues. One note would be that I think the APL processor only supports 1.8V I2C and the USB2ANY only supports 3.3V I2C by default, so a level shifter (or disconnecting from the processor) may be necessary. Alternatively, you can replace the 3.3V LDO in the USB2ANY with a 2.5V LDO or external power supply and then disable or remove the pull-up resistors to prevent 2.5V on the APL I2C pins. I would expect it to be a little less reliable at detecting 1.8V as a logic level high, but I never saw any problems when doing it this way in the past.