Other Parts Discussed in Thread: UCC28C43
My customer are using UCC28C43-Q1 for EV/HEV PTC application.
specs: Flyback isolation application
Input: 150-500V DC.
Output: 15V/0.33A=5W.
Now my customer want to add input over voltage protection, when input beyond setting value, controller can disable MosFET driver and IC don't need working,
But UCC28C43-Q1 don't have over voltage function , Is there any suggestion for it?