Other Parts Discussed in Thread: TINA-TI, TPS62147, TPS62148, , TPS62136
Dear Support team,
Could you please let me confirm some points when using this TPS63140 as a inverting back boost converter discribing in Application Report SLVA469C.
We assume that the converter will be used under the following conditions.
Conditions :
* Vin: 5V ~ 9V
* Vo: -6.02V (or -6.4V)
* Io = 10mA (Inrush: 90mA)
* Tj: -10 ℃ ~ 75 ℃
* Is it possible to use TPS63140 as inverting back boost with this condition as like description in SLA469C?
* Behavior when using beyond the output voltage range
The recommended operating range on the data sheet is -6V as Vout (max), but can it be used at -6.02 to -6.4V? Will it affect performance? (Absolute max rating is defined as 7V)
* Output voltage accuracy
Since the voltage setting method is the same as that for the step-down converter, can the output voltage accuracy be considered the same?
* Can the Discharge function be used?
* When I tried to simulate the inverting buck-boost circuit in datasheet p.27 with TINA-TI, no output voltage was obtained.
Is such a simulation impossible?
Best Regards,
Hirokazu Takahashi