Part Number: LP5912-Q1
Other Parts Discussed in Thread: LP5912
Current capability value of LP5912-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Aishwarya S1,
The LP5912 is rated for use up to 500mA:
Please note, the ability to support 500mA of load current is a function of the thermal performance., The power dissipation is (VIN-VOUT)*ILOAD.
The power dissipation times TJA can help to estimate the die junction temperature.
I hope this answers your question.