If the class resistor does not match the load, is the PSE supposed to shut down the power to the PD?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the class resistor does not match the load, is the PSE supposed to shut down the power to the PD?
Hello Tyson,
Table 1 in the datasheet defines the values for the class resistor. It does not relate to the load, but to the IEEE802.3 standard.
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments
But according to Table 1 the class resistor corresponds to a minimum power at PD and a maximum power at PD. Suppose the class does not correspond to the range of minimum to maximum power. For example suppose the class resistor is 243 Ohms which corresponds to a class 1 but the load is 100 ohms which would draw 25 Watts at 50 Volts which is a class 4. Does the PSE shut off the power. Similarly suppose the class resistor is 63.4 Ohms which is for a class 4 but the load is 833 Ohms which would draw 3 Watts at 50 Volts which would be a class 1. What does the PSE do?
Hello,
It is hard to say for ALL PSE's, but I will explain for IEEE 802.3 compliant PSE's.
If the power consumed by the PD is less than the class the PSE will continue to power the device. If you look at any of our test results for a design, you will see we check efficiency, startup and load regulation at multiple load levels (starting from no load to full load).
If the power consumed by the PD is more than the class allocation, then the PSE will shut off power.
In the new IEEE802.3.bt standard, there is also something called power demotion, which is explained in this video:
https://training.ti.com/understanding-power-demotion-tis-ieee8023bt-powered-devices-pd
If this post answers your question, please indicate so by marking this thread as resolved. Thank you.
Regards,
Michael P.
Applications Engineer
Texas Instruments