This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC59208F: what are the key difference between TLC59108F and TLC59208F

Part Number: TLC59208F
Other Parts Discussed in Thread: TLC59108F, , TLC59108

Hello Community,

i would like to be sure of the differences between TLC59108F and TLC59208F.

This E3E topic describes
that the difference between TLC59108 and TLC59108F are just the output structure. (Current-Source / Open-Drain)

that is Open-Drain for both.
HW wise i found

parameter TLC59108F TLC59208F
Maximum Output Current 120mA 50mA

the Functional Block Diagram is also about the same for both:

the only other difference found is with Regular I2C Bus Slave Address:

there fore the TLC59208F has much more possible addresses.

are there any other differences i missed?

and are the three parts (TLC59108, TLC59108F, TLC59208F) interchangeable from a I2C view?
(so i can switch the parts later if needed but don't need to change software?)

thanks for any feedback!

sunny greetings
stefan