TPL7407LA is a driver ic with 7 outputs. The current rating per channel they have mentioned 600 mA per channel but maximum current output mentioned is 500 mA. As it is having 7 outputs if we connect all outputs
in parallel the maximum output current is 7*600 mA=4.2 A.
So my question is the maximum output current when we connected all outputs in parallel is 4.2 A or 600 mA.
Please reply as early as possible.