This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73601-EP: Radiation report

Part Number: TPS73601-EP
Other Parts Discussed in Thread: TPS73801-SEP

Hallo,

Is there radiation related (TID or SEE) test reports available for TPS73601MDCQREP. I could find a SEE report for TPS73601MDBVREP. Both are different packages.  Along with this i am attaching the report which i got . Kindly provide me the report, if you have for the required one.

Thanks and regards,

VijiTPS73601see test from texas instruments.pdf

  • Viji,

    We do not radiation test our commercial or EP variants of our devices.  The SEE report you reference is not endorsed nor generated by TI.

    TI cannot share wafer, die and process details specific to any device, as this information is proprietary. Typically there are differences between space and non-space devices (including Military and EP grade products). These differences can be in the form of process, layout, or design changes. These are done to improve radiation performance of space device. Please note that radiation performance for a non-space device can be significantly worse compared to space qualified device even though electrical performance is identical. In addition there are several factors on non-space device that makes it risky for space applications. Some of important factors:

    -          No single controlled baseline: Translates to high variability of radiation performance (commercial products)

    -          Mostly use copper bond-wire: May not be reliable for space environment (commercial products)

    -          No testing for radiation at lot level: High risk of getting devices that have poor radiation level (non-space products)

    If you require radiation qualified components, we do offer a lower cost space enhanced qualified TPS73801-SEP LDO with radiation characterization.  It is a wide Vin LDO.

    If this answers your question, please click "This Resolved My Issue"
    Regards,
    Wade