Other Parts Discussed in Thread: TPS54428
Hi support team,
I have a question about TPS54228.
The output voltage of TPS54228 can be set by R1 and R2 according to equation (3) in the datasheet.
What is the behavior of the output voltage if the combination of R1 and R2 is set so that the output voltage exceeds 7 V?
For example,
where VIN = 18 V, R1 = 8.25 kΩ, and R2 = 221 Ω,
the calculation will be VOUT = 29.3 V.
How does an actual IC behave?
I want to know the operation of the IC as a case study if the value of R2 is incorrectly mounted.
This is because I want to consider concerns about whether overvoltage will be applied to the subsequent circuit.
Best regards,
M. Tachibana