Other Parts Discussed in Thread: TPS610986,
Hello
I used both the TPS610986 and TPS61291 boost converter in order to power a load that consume around 200mA in both situation (TPS610986 powering the load then use the TPS61291 to power the same load) the boost converter voltage drop down to around 0.45V. Both of them work correctly with load that consume 10-20mA but with higher load the voltage drop down i didn't understand the reason as the datasheet mention that both could work fine by supplying 200mA. ( I also tried a load that consume 100mA but i faced the same problem)
Input voltage: 3V I also used 2V
Output voltage: 3.3V
Could you please tell me how to fix it.
Thanks
PS: attached the schematic of both boost converter that I used