This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21040: slow charging application - alternative device without safety timer?

Expert 6470 points
Part Number: BQ21040
Other Parts Discussed in Thread: BQ24041, BQ24086

Team,

we would need a standalone charger like BQ21040, but without the safety timer - we have a limited power source and need to limit charging current down to 20-30mA, so it will take more than a day to recharge battery (while the safety timer is fixed for 10h).

Also, we checked BQ24041 (no timer), but it has an Enable pin instead of TS pin, while we need to have both of these pins (just without safety timer). 

What can you propose?

Thank you.