Other Parts Discussed in Thread: LM5022
Hi,
I'm designing a flyback using the LM5022
VIN: 30V to 600V
VOUT: 15V 2W
- CH1: VGS Q102 (principal sw)
- CH2: VAK D4 (output diode)
- CH3: VDS Q102
- CH4: iDS Q102
2 questions:
- VIN=400V, LOAD=103R0. the inrush current at the turn ON of the MOS is principaly due to transformer capacitance ? So to limit the peak current, a "new" winding is recommended... any suggestion ?
- I'm not able to have a stable PWM at low voltage (i.e. 60V), is there a "clean" way to select components to avoid this ? I think it's start with a good slope compensation.