Dear Sir/Ms.
Customers use TPS61199 to design Back light LED Driver. After the experiment, it was found that sound was generated, and the output capacitance was found to have an effect.
TPS61199 Vin is 12V
Panel Specifications
LED String Current 70mA (Typ.) 77mA (Max.) Note: 4 strings and 7pcs LED of one string
LED String Voltage 19.6V (Min.) 21.7V (Typ.) 23.8V (Max.)
The customer's product issue has been resolved.
But the manager of RD wants to know why this is happening? The customer has removed the E-CAP, the MLCC has increased the test, and still has a voice. Is there any hat can explain the difference between E-CAP and MLCC as output capacitors?
Attached is experimental data.
Best Regards,
Kami Huang