Other Parts Discussed in Thread: TPS3808
We would like to change the Rsense to a higher resistance as below to decrease the current consumption, could you please help check if it is workable or is there any risk?
R2260 => 1.8Mohm
R2261 => 140kohm
R4330 => 1.8k
3.5~16V input and the resistance is 1.8M +0.14M+0.0018M=1.9418M
The current will be 3.5V~16V /1.9418=1.80uA ~8.23uA .The leakage in ISENSE pin is 25nA. Could you help check is there any risk?
A further question: What is the acceptable range we can increase the resistance?