Other Parts Discussed in Thread: UCC28730, TL431
Tool/software: WEBENCH® Design Tools
I'm trying to find suitable components for a 85-440VAC automotive flyback converter, with a single +12V/0.6A output. The Webench power designer suggested various designs based on the following parts:
- UCC28C4x,
- UCC2813-x,
- or UCC28730 (not suitable because of the 700V startup switch!?)
The AN-22 application note from Power Integrations Inc. states that the output regulation (error) depends on the feedback technique. For example:
- Primary regulated: +-10%
- Opto/Zener: +-5%
- Opto/TL431: +-5%
What output error should be expected when using current-mode PWM controllers such as the ones mentioned above?