Hi,
I am designing a new circuit based on BQ24050 Texas Instruments Li-Po Charger. The battery that the system uses doesn´t have NTC, it only has two pins (+ and -). My question is, How should I connect the TS pin?
Based on this post e2e.ti.com/.../762756 and that the battery will be permanently connected. I think that my options are:
1. Connect TS to GND with 10k resistor
OR
2. Connect TS to GND with 237K
OR
3. Use an external NTC (i don´t like this idea)
Also, I am not sure if I should connect the TS to the host microcontroller to command the IC charger because my battery doesn´t have NTC.
Best regards,
Carlos