Hi all,
We're developing a 24VAC to 24VDC, 4A converter using the LMR14050 ICs.
To test the circuit we've built a prototype on breadboard. At low output currents, the circuit performs well however, when we apply a load > 2A the LMR14050 catastrophically fails. We've destroyed 8+ ICs trying to figure out what we've done wrong.
Attached is the circuit we've used from Webench. Note, the circuit didn't work with Cff in place so this was removed.
Any input would be greatly appreciated.
Cheers,
Chris.