This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPIC74100EVM: Vout drop when Vin is adjusting & Vout couldn't be generated when Vin < 4.7V

Part Number: TPIC74100EVM


Hi Team,

I have two questions of using TPIC74100EVM.

1. Vout drop when Vin is adjust from 5V to 6.5V. It happened in Vin is about 5.8V. the switching is changing from Q1/Q2 to Q3/Q4, the drop voltage is about 200mV. Could I add some components to eliminate the drop voltage? 

2. Vout couldn't be generated when Vin < 4.7V, the feature of datasheet said the Vin could operate when Vin = 1.5V-40V, could I set some pin to let IC could work in 1.5V-40V?

ps. I add Vin in C5/C6 of EVM.

Regards,

Roy