This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25886: Charging current lower then the set value

Part Number: BQ25886

Hello everyone,

This is my problem. I am using BQ25886 for building a USB powered charging circuit on my device. I have a 2 cell Li-ion battery with 7.4 V nominal voltage. The measured charging current is 750 mA instead of the set value of 1.2 A. I am using several different wall adapters with maximum output current of 2.4A.

I am attaching the schematics of my charging block.

The input current is set to the maximum value of 3A via shorting ILIM pin to GND (R15 = 0 Ohm).

The charging voltage is set to 8.2 V via shorting VSET pin to GND (R16 = 0 Ohm).

The charging current is set to 1.2A (R17 =4k7)

Since I am not using a thermistor, I connected the TS pin to a voltage divider, that sets the TS voltage to 50% of the REGN voltage. According to page 9 from the datasheet, this voltage should be between 45 and 68 % of VREGN in order to have a full charging current. I tried also the divider configuration from page 21 (R24 =4.7k, R25 =27k in parallel with 10k, resulting in TS voltage =60% of VREGN) and the charging current was still 750 mA.

Additional information is that I have the data lines of the USB connected to an FTDI USB to UART translator chip. However, disconnecting the FTDI didn’t fix the charging current.

I have tried also to bypass transistor T3 from my false polarity protection circuit but it had no effect neither. Instead of the fuse R14 I have a 0 Ohm resistor.

I hope my description of the schematics and the issue is detailed and clear enough. I am looking forward for any ideas and suggestions. Thank you in advance.

 

Best Regards

Angelo