This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160A: TPS54160A

Part Number: TPS54160A

Hi, Team

I calculated values on based the equation (48)~(50) for the typical application of the datasheet.
Vout=3.3V, Gmod(fc)=0.542, gm(EA)=97uA/V, VREF=0.8, fp(mod)=1.5kHz, Cout=47uF, RESR=10mΩ
The result is following;
- Rc=3.3/(0.542*97u*0.8)=78.46kΩ (76.2kΩ)


- Cc=1/(2π*78.46kΩ*1.5kHz)=1352pF (2710pF)


- Cf=47uF*10mΩ/78.46kΩ=5.99pF (6.17pF)


The values inside the parentheses are the result of the datasheet.

Cc=1352pF or 2710pF
Which is correct?

When I replace '2π' with 'π' in the Cc equation i got the result same as mentioned in the datasheet. So i am little bit confused which formula to use for calculating Cc.

Etheir Cc=1/(2π*78.46kΩ*1.5kHz) = 1352pF  OR  Cc=1/(π*78.46kΩ*1.5kHz) =2705pF

Thanks and Regards,
Juzer Tarwala