Other Parts Discussed in Thread: TPS92691, TPS92692
I'm designing a power led driver. The white led array is composed by 20 parallel rows each row with 10 led in series. Total current 6A and array voltage 34 V. I need to dimmer the light with external digital PWM signal.
I found 3 IC:
TPS92690
TPS92691
TPS92692
My question is
TPS92690 is a controller, so the current depends on external components, so why in the datasheet the description says that is suitable for currents up to 5A, where is the limitation?
This controller uses only 1 MOS for current control, there is no PWM mos on the load. Why?
TPS92691 uses 2 MOS instead of only one of the TPS92690: Is it a better solution?
TPS92692 uses an High side PWM P channel MOS instead of a Low side N channel PWM MOS: what is the advantage of this solution?
Thank You