Hi team
Regarding the protection, does TPS562201 have OCL, UVP and thermal shut down ?
And are each behaviors below ?
Is the below correct ?
- OCL
- Monitor low-side FET drain to source voltage.
- If over current is detected, low-side FET keeps on until less than OCL level. (2.4A – 4.0A)
- If TPS562201 recover from OCL, high-side FET turns on from after next cycle.
- UVP
- If UVP is detected, TPS562201 is shutdown at typ 24 us, and then restart after hiccup time at typ 15 ms
- What is hiccup wait time of typ 1.8 ms ?
- Thermal shutdown
- If the temperature exceeds typ 160 degree, TPS56201 is shutdown.
- How to recover shut down mode ?
Thank you and best regards,
Michiaki