This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63805EVM-026: Changing the input voltage

Part Number: TPS63805EVM-026
Other Parts Discussed in Thread: TPS63805

Hi, I am using the TPS63805EVM evaluation board. I configured the output for 4.9V at 1A, and my input is a 3V power supply. The board was working well until I turned my power supply down from 3V to 2.5V. Once I did that, the board stopped working and even with no load on the output, all of the power sent to the input of the device goes to ground and does not regulate the output at 4.9V. Do you know what I did wrong? Thanks