Other Parts Discussed in Thread: BQ24040, BQ25125
Hey guys.
It seems BQ25010RHLR is not recommended anymore. I was working on a USB charging + CC2640R2 wireless application.
The battery I'll be using is www.adafruit.com/.../258
Lithium Ion Polymer Battery - 3.7v 1200mAh
I need to charge this via micro USB cable and Integrated USB Charge Control with 200mA Charge Rates or above is acceptable.
Just like the BQ25010RHLR, I'm looking for an IC that has a DC-DC buck converter;
for instance, I used BQ25010RHLR and created 3V from the integrated buck converter.
Status pins from the BQ chip are required to check the charging status.
The size and price won't matter but I don't like ball grid chips.
In this case, what are the alternatives?