Hi Team,
Our customer would like to confirm if the TPS61028 :
-Is the EN pin on the TPS61028 does not have clamp diodes since the absolute max specs say it can take –0.3 V to 7 V?
-If the above answer is yes, will there be no voltage present on the VBAT and SW pins but there is a logic level signal on the EN pin that current will not be consumed by the EN pin?
Please let me know if you need more information from the customer.
Thanks!
Jonathan