Other Parts Discussed in Thread: USB2ANY
Hi Team,
Our customer is having trouble below to configure the default Vref voltage of the device TPS65400 regulator in hid customer board using the Fusion Digital Power Designer tool
1. TPS65400RGZR IC employed on one of the design boards reads a wrong I2C address for a resistor value of 82KOhm.
2. The default Vref voltage is 1.355V instead of 0.8V. I did try to program the IC to default values but of no use though the tool fusion digital power designer tool says successful in storing to NVM.
Here's what the customer has done to configure TPS65400 VREF:
- connect the device, the tool recognizes the device with the right I2C address
- then customer click on the option - click to configure device followed by changing the write protect mode to 0X00
- change the Vref to what's required- write to hardware and then store config to NVM
- It says saving device config(RAM) to flash memory
- but customer sees the default value even post configuration of the device
Let me know if you need more clarification with the customer inquiry.
Thanks.
Jonathan