Hello everyone!
I am using a BQ25618EVM charger IC for Li-ion battery charging. While testing the IC using an electronic load instead of a battery and setting the input current via the EV2400 I2C interface, I found that when I set the charging current to 60 mA using BQStudio, the measured current supplied to the electronic load is 80 mA. This trend existed even when I increased the current until 160 mA. However, upon increasing the current beyond 200 mA, the measured and set current values matched again. Also, when I set the current to 40 mA, the measured current was recorded as 40 mA.
I have multiple units of BQ25618EVM and I found this issue only with 2 out of 10 units. Also, I tried testing these ICs again using actual batteries and the same trend existed. Moreover, I checked the startup register settings of this IC, and it matched the default settings mentioned in the BQ25618 IC datasheet.
So why is the measured current different than the set current in some of the ICs? Please let me know how I can troubleshoot this issue.