Hi Sir,
My customer recently encountered a problem with TPS51225C (generating 3.3V and 5V from 12V).
The output voltage increases about 0.8~1V as the temperature rises from 25 degree to 60 degree.
They have checked the following items but found nothing anomaly.
1. The voltage level at VFB1 and VFB2 - > Stable and no deviation
2. The voltage at VIN of IC and synchronous mosfet -> Stable
3. The phases at SW1 and SW2 -> Stable and no obvious jitters as temperature rises.
4. The voltage at VREG3 and VREG5 ->
As the output voltage increases with temperature, the voltage at VREG5 rises too (switchover) while the voltage at VREG3 does not change too much (about 3.4V)
It would be kind of you to give us some directions.
Thanks
Sincerely,
Edward