Other Parts Discussed in Thread: TPS61022
Dear TI Team,
If the difference between the input voltage and the output voltage of the TPS61236P is designed below 0.5V, can you know what kind of damage it does to the IC?
VIN: 4.2V
Vout: 4.5V 1A
In the above design, short defects of SW pin and VOUT pin occur about 5%.
(Chip Only Impedance SW to VOUT pin: about 22ohm)
I want to check if the cause of the defect is due to the voltage difference between Vin and Vout.
Best Regards,
Thanks.