Other Parts Discussed in Thread: LM5176, LM5001, TPS55340
Hi
I consider using a LM5176 with an input voltage down to 3.6V and it will therefore need a 9V bias voltage. For this task TPS55160-Q1 was suggested but the issue with this part is that the max input voltage is 36V and the abs. max. is 40V.
But in my application we have the following specifications:
Nominal Input voltage: 3.6 to 36V
Input overvoltage TVS protection = TPSMA6L36A: VbrMax = 44.2V @ It = 1mA
Output voltage: 9V
Output current: 4mA
Ambient temperature: The board will be mounted inside a box with no air flow and the temperature inside the box is estimated to be up to about 83C and down do -40C.
The building height should be kept below 4mm where possible, and the absolute max building height is 8 mm.
If You have any suggestion for a similar part that can handle higher voltages, it would be a big help.
Best regards
Klaus