This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92640: Do you have any reference design to use TPS92640 with about 400V output for many LED driving in series?

Part Number: TPS92640
Other Parts Discussed in Thread: UCC28810, TPS92075, LM3444, LM3445

 Hello guys,

 One of my customers is looking for a reference design which can drive many LED in series with about 400V output using TPS92640 (Buck converter type LED driver).

 The LED current is 150mA~300mA as type 1 and about 2A as type 2.

 If you know any schematic or reference design using other device, could you please tell me it?

 Your reply would be much appreciated.

 Best regards,

 Kazuya.