rt Number: PTH08T250W
Hi, everyone,
I have design a power sequence circuit, but I am not sure that the design is correct or not, plz help me to check, thanks a lot
Here is my thought :
I use 3 TL7712As to control 3 PTH08T250Ws (3 sets controlling circuits),
first one TL7712a pin5 connect to PTH08T250W Pin20, TL7712a set delay 1.3ms (the second picture),
second and third objects are designed the same, but Ct (delay setting) are 28.6ms and 61ms (show second picture, but Ct values are different, Power modules' output power different).
Power module output voltages are different, but in range 0.7~3.6V
I think PTH08T250W Pin20 (Track pin) to up are like this below, it is controlled by TL7712A (which is 12V voltage supply, delay time are 1.3ms, 28.6ms, 61ms),
Track pin (PTH08T250W Pin20 be active needs 20ms)
I hope my design is correct, thanks