Hi,
1. Are I can feed each PVIN from other voltage (suppose PVIN1=12v, PVIN2 and 3 = 5v)?
2. If yes, Are device need a power sequencing between PVIN1, PVIN2 and PVIN3? What is the recommended power sequencing?
Thanks
Naftali
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
1. Are I can feed each PVIN from other voltage (suppose PVIN1=12v, PVIN2 and 3 = 5v)?
2. If yes, Are device need a power sequencing between PVIN1, PVIN2 and PVIN3? What is the recommended power sequencing?
Thanks
Naftali
Hi, Naftali
1. Yes, you can, PVIN1/2/3 can be connected to different input rails. And VIN pin can be connected to 5V or 12V.
2. Suggest to enable Buck1/2/3 converter after PVIN1/2/3 voltage power on.