Hi Team,
Is there any slew rate limitation on the TPS62160-Q1 VIN pin? There is another DC/DC converter that feeds the TPS62160-Q1 with a very fast turn-on, and I want to make sure that will not impact the TPS62160-Q1 VIN..
Thank you!
Jared
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Is there any slew rate limitation on the TPS62160-Q1 VIN pin? There is another DC/DC converter that feeds the TPS62160-Q1 with a very fast turn-on, and I want to make sure that will not impact the TPS62160-Q1 VIN..
Thank you!
Jared
Hello Amod,
The voltage at the VIN pin is from 0V to 3.3V in <1ms. Will that be acceptable? The EN pin is supplied by 1.8V from a different source.
Thanks!
Jared
Hi Jared,
There is no limit as such on the slew rate so the 3.3V in 1ms or lower is acceptable. Curious to know why you are using a 17V rated device for a 3.3V input?
Regards,
Amod