This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2818A-Q1: MOSFET selection and Power loss with given gate resistance

Part Number: UCC2818A-Q1
Other Parts Discussed in Thread: UCC2818

HI TI,,

Please help me to get the correct gate resistor and mosfet for the UCC2818A-q1 because as given picture you are using 20E resistance which is source of switching loss .my spec is AC 85 to 265 and out 390V 750W (1.92Amp). so if i calculate the power loss I^2x R loss with a mosfet the conduction loss is less (0.44W) but while calculate the switching loss with 100Khz switch frequency it is 26W which is very high with 20E resistance.

Can you please let me know the gate resistance value which i should use.

i am using below formula to calculate the switching loss : MOSFET part Num : STWA30N65DM6AG

i peak :13amp

Vds: 390V

Fw :100Khz

Tch: 50n