We are looking in confirmation of the circuit correctness which is requested by seniors. Kindly do the needful if anymore information required feel free to ask.
Input supply is with in the module, which can support 3.3V @ 2A,
Case1:
Vout for VDD_1V8 required is 1.8V, Iout required is 0.1A, Expected voltage ripple not more than 20mV.
Case2:
Vout for VDD_1V2 required is 1.2V, Iout required is 1.0A, Expected voltage ripple not more than 20mV.