Other Parts Discussed in Thread: LM5134
Hi Team,
My customer is evaluating LM5034, and has a question about VIN pin application. The LM5034 datasheet shows applications information for VIN at page 19. There is the "Figure 26. Input Transient Production". The circuit of the figure 26 be used to suppress transients which may occur at the input supply. They understood that. But, they have a question if the LM51034 has any limitation of slew rate to the VIN input voltage. Because there were some power supply control ICs that could malfunction at high-speed dv / dt with an IC Vin of 20V / ms or more, so they were wondering if VIN application of LM5034 was the same intention.
Thank you.
Best Regards,
Koshi Ninomiya