On the bq24156A, what is the purpose of the Charge Current Sense Voltage [LOW_CHG], and what significance does 22.1mV have?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
On the bq24156A, what is the purpose of the Charge Current Sense Voltage [LOW_CHG], and what significance does 22.1mV have?
In the I2C register, there is a bit called LOW_CHG which forces the charge current to 325mA. To get this current, the voltage across the Rsense resistor is regulated to 22.1mV. The default setting for the LOW_CHG bit is '1', which means that if one wants to charge with more current, this bit must be set to '0'.