This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: What is the best way to limit the current on the output?

Part Number: UCC28950
Other Parts Discussed in Thread: PMP8740, , UCC28951-Q1, TL431

Mine schematic looks like this for the PSFB converter.

PSFB converter schematic.pdf

I saw a reference model from PMP8740, see this schematic. 

PMP8740 2KW Rev_E Full Bridge - Schematic.pdf

I also read the datasheet/document of this model but I still don't understand how much current they are limiting? 

I need to make a design that can charge a battery of 8kWh with 500W-2000W (so with 0.0625-0.25C). So when I connect the PSFB converter with the battery I need to choose a limit with my microcontroller.

What is the best way to limit an adjustable output current with a microcontroller.

More information over system:

Output votlage: 43.8V need to stay constant to charge a battery of 36-43.8V 

Output current max load: 45.6A (2kW)

Battery is 8kWh.