This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am testing the design that was provided by our contractor of the TPS40077.
The input is 6.5V to 9.5V and is supposed to give 3.3V output, but I am only getting 1V.
Have you been able to make the changes Yuchang Zhang suggested?
Have they addresses your issue?
The TPS40077 controller uses the KFF pin to provide UVLO, Voltage Feed Forward and a maximum duty cycles. The low resistance on the KFF pin (10k) would create a very low maximum on-time, which is likely the cause for your 1V output.
The 100kOhm value Yuchang Zhang provided you with is for a 4.5V UVLO, since your minimum input voltage is 6.5V, you may want tp select a resistor as high as 140kOhms for a UVLO voltage closer to 6.5V. Also, since the KFF resistor programs the voltage feedforward gain, you should review the compensation design using the design tool - https://www.ti.com/lit/zip/sluc263
TPS40KType III Loop Stability kVenable_sluc263c-071312_ChrisJensen.xls