Other Parts Discussed in Thread: LM25117
Hi Sir
This is our main power circuit. The LM3488 does not meet reference design 5V,10A output, and our design target is 5V, 5A.
Due to my power supply capacity, the E load set at 1.5A. The current load and voltage position are set on C432 .
All of input is 1.5A current load, the variable is input level 6V, 10V, 12V and observes C432 output voltage. We also short the R422.
- 6V input, 5V output is OK
- 10V input, 5V output drop.
- 16V input, 5V output drop.
Please help us to find out the output drop issue.